Technical FAQs

Ask a Question

Can I connect SW & XW inverters to a single SCP?

Issue:
Can I connect SW & XW inverters to a single SCP?

Product Line:
Conext SW/XW hybrid inverters

Environment:
Connecting different systems with one single Control Panel

Cause:
Due to the difference in features and firmware, connecting two different model inverters in the same system would give programming errors. With two inverters in the system, they will need one master only and if these two systems don't have a common output this would stop output production on slave system.

Resolution:
Having an SCP per Inverter system would be ideal but if only one SCP is available you can try switching between units when configuration is needed.
Was this helpful?
What can we do to improve the information ?