Technical FAQs

Ask a Question

Can I connect SW & XW inverters across models in the same system?

Issue:
Can I connect SW & XW inverters across models in the same system?

Product Line:
Conext SW/XW hybrid inverters

Environment:
Trying to connect different model inverters in the same system

Cause:
Due to the difference in features and firmware, connecting two different model inverters in the same system is not an option. Making this connection may come with communication issues between these inverters as well as a possible sync issues.

Resolution:
When using multiple inverters in the same system use the same model to ease functionality.
Was this helpful?
What can we do to improve the information ?