Technical FAQs

Ask a Question

Is there a programmable version of TP-1011 thermostat?

Issue:
Is there a programmable version of TP-1011 thermostat?

Product Line:
Thermostats

Environment:
Application

Cause:
Replacement

Resolution:
The TP-1011 is a very old type control stat. There is NO new version that is programmable or even digital. To upgrade, would require updating the building controls with our BMS system.
One of our local Partners would have to be contacted, to see what would be needed for upgrading .
Was this helpful?
What can we do to improve the information ?