Technical FAQs

Ask a Question

Do XVBC9B alarm units trigger when a light is activated?

Issue:
XVBC9B operation

Product Line:
Tower Lights and Beacons

Environment:
XVB—70 mm Diameter

Resolution:
XVBC9B alarm units is independent from the lights. It uses it's own circuit to be triggered.
Was this helpful?
What can we do to improve the information ?