Technical FAQs

Ask a Question

Will the linkage kit AV-391 work with a VB-9323-0-4-11 valve body, or any 2" VB-9XXX series valves, using a MP-371 Actuator

Issue:
Will the linkage kit AV-391 work with a VB-9323-0-4-11 valve body, or any 2" VB-9XXX series valves,  using a MP-371 Actuator 

Product Line:
OBS VB-9XXX 2" Valves 

Environment:
Maintenance

Cause:
Installation 

Resolution:
No , MP-371 actuator  Linkage Kits are the AV-391 linkage kit for VB-7XXX 1/2" - 2"  Valves  ;  AV-391 linkage kit is for VB-9XXX 1/2" -1-1/4" Valves ; 
AV-392  for VB-9XXX 1-1/2" - 2" valves , see attached Instruction bulletin for Linkage
Was this helpful?
What can we do to improve the information ?