Technical FAQs

Ask a Question

Why the GT500MVX kept stuck in the wake-up mode?

Issue:
DC contactor closed then the AC contactor closed then immediately the AC contactor opened. It will then repeat this process repeatedly. The display would said wake up mode.
 
Product Line:
GT500MVX
 
Environment:
 
Cause:
Possibly bad K1
 
Resolution:
Press F1 and see if the fault can be clear. If not, try to cycle the power to the inverter and see if the fault clear. If it does not clear then contact us at 866-519-1470 option 3 & 3.
Issue:
DC contactor closed then the AC contactor closed then immediately the AC contactor opened. It will then repeat this process repeatedly. The display would said wake up mode.
 
Product Line:
GT500MVX
 
Environment:
 
Cause:
Possibly bad K1
 
Resolution:
Press F1 and see if the fault can be clear. If not, try to cycle the power to the inverter and see if the fault clear. If it does not clear then contact us at 866-519-1470 option 3 & 3.
 
Was this helpful?
What can we do to improve the information ?