Technical FAQs

Ask a Question

How to Order the Top Cover Part # NHA54183 for EX Transformers in MYSE?

Issue:
Need to Order an EX Transformer Enclosure Part like the Top Cover (NHA54183), but not Recognized in Q2C or MYSE.

Product Line:
Transformers

Environment:
EX Low Voltage Distribution Transformers

Resolution:
Enclosure Parts (Replacement Parts) like NHA54183, NHA54182, NHA96044 etc. have not been loaded into the order system as yet. Distributors need to request them as a special item from their Local Sales Office. The Local Sales Office will then quote the Catalog number. This will be the process until such time as Enclosure Parts (Replacement Parts) are loaded into the system.
Was this helpful?
What can we do to improve the information ?