Technical FAQs

Ask a Question

What is the current part number for a VB-7223-000-4-8 valve, or any VB-7000 Series valves with 000 actuator code ?


Issue:
What is the current part number for a VB-7223-000-4-8 valve? 

Product Line:
Field Devices 

Environment:
Ordering

Cause:
Part number clarification

Resolution:
A recognized valve part number to order is VB-7223-0-4-08
Was this helpful?
What can we do to improve the information ?