Technical FAQs

Ask a Question

Does the ATV320 allow you to setup 3-wire control and Fast Stop?

Issue:
Does the ATV320 allow you to setup  3-wire control and Fast Stop?

Product Line:
ATV32  ATV320

Issue:
compatibility of functions

Environment:
All

Resolution:
Yes, tested this in SoMove software and the ATV320 allows both.  There is nothing in the programming manual's Compatibility Table that states otherwise.
Was this helpful?
What can we do to improve the information ?