Technical FAQs

Ask a Question

Where is the the UL Sticker or Label located on a NEMA Enclosed Full Voltage Starters and Contactors?

Issue:
Where is the UL marking located on an Enclosed NEMA Starter or contactor? 

Product Line:   
NEMA Style, Full Voltage Non-Reversing and Full Voltage Reversing Starters and Contactors Class 8502 & 8702 8536 & 8736 8538 & 8738 8539 & 8739 8903L & 8903S 8903 8910, 8911, 8965 8940 8941

Environment:    
US Product

Cause:   
Specifications

Resolution:       
The UL marking is on the product itself inside the enclosure.  Once you remove the cover or open the door, it's on the red nameplate on the product.
Was this helpful?
What can we do to improve the information ?