Technical FAQs

Ask a Question

What is the part number for a 30A 3 pole breaker feeder bucket for a Model 5 or Model 6 MCC?

Issue:
What is the part number for a Model 5 or Model 6 30A feeder bucket for a Motor Control Center?

Product Line:
Motor Control Center

Environment:
Model 5 or Model 6 MCC

Resolution:
Both the Model 5 and Model 6 MCC's accept the same feeder buckets. The model 5 MCC will require a midshelf as well which is part number
8045086550. For a 6" Feeder bucket the part number is 8998HBF030 and for the 12" standard bucket it is 8998SBF030. 
Was this helpful?
What can we do to improve the information ?