Technical FAQs

Ask a Question

What is the voltage limitation on the BMXFTW301

Issue:
Can I use the BMXFTW301 cable on the AC I/O cards?

Product Line:
X80 , M340, M580

Resolution:
The voltage limitation on the BMXFTWxx1 cables is <= 48V.
Was this helpful?
What can we do to improve the information ?