Technical FAQs

Ask a Question

If you are controlling the R2 relay over the network what happens to the relay status if you lose the network after writing to turn it on. 

Issue:
What happens to the ATV61 or ATV71 relay status if you are controlling R2 relay over the network and you lose the network?

Product Line:
All 

Environment:
ATV61 and ATV71 drives

Cause:
All 

Resolution:
If you write and turn on the R2 relay and you lose the network the relay will remain in that state until your write to turn if off or power down the drive. 
 
Was this helpful?
What can we do to improve the information ?