Technical FAQs

Ask a Question

SoMove displays "Update of identification parameters failed." when trying to connect to an altivar drive.

Issue:
SoMove displayes "Update of identification parameters failed.' when trying to connect to an altivar drive.

Product Line:
SoMove

Environment:
All models, All serial numbers.

Cause:
Conditions to connect SoMove not met.

Resolution:
In order to connect SoMove to a drive, the drive must be at RDY or NST state (0.0 for an ATV212 series).  If the drive is in a run state or has a run command connected, SoMove will not be able to start.

 
Was this helpful?
What can we do to improve the information ?