Technical FAQs

Ask a Question

How is the CP-9301, CP-9302 Actuator Drives powered?

Issue:
How is the CP-9301, CP-9302 Actuator Drives powered?

Product Line: 
Valves and Actuator

Environment:
Maintenance

Cause:
Application assistance

Resolution:
The CP-9301 Actuator Drive is powered by the actuator, with the actuator supplying the drive the necessary voltage .
  • 24/120/240 VAC
  • 3% of Input Span
  • Factory Preset 6-9 VDC
 
See Instruction bulletin for further details
Was this helpful?
What can we do to improve the information ?