Technical FAQs

Ask a Question

What is the length of the LV426932 shaft?

Issue:
Looking for length for the LV426932.

Product Line:
Powepact Breakers

Environment:
B Frame Breakers

Resolution:

The dimension that is important is the distance from the back of the breaker to the front of the panel door. That dimension for the LV426932 is 7.87 inched minimum and 23.62 inches maximum. See the instructions in document EAV91029.
Was this helpful?
What can we do to improve the information ?