Technical FAQs

Ask a Question

How can I change the IP Address on an ATS48?

Issue:
Customer has an ATS48 and wants to change the IP Address to continues controlling over Ethernet.

Product line:
ATS48, Altistart 48

Environment:
all

Cause:
Communications

Resolution:
The ATS48 only has Modbus built in.  If they are using Ethernet to control, this will be via an external Gateway.  The ATS48 only offers Modbus communication parameters to be adjusted:
- Address
- Communication speed (baud rate)
- Format (Parity)

 
Was this helpful?
What can we do to improve the information ?