Technical FAQs

Ask a Question

What is the range of the Nominal Motor Current for an ATV66 series drive?

Issue:
What is the range of the Nominal (motor) Current setting of an ATV66 series drive?

Product Line:
ATV66 series drives.

Environment:
All models, All serial numbers.

Cause:
Drive is being used on an undersized motor and the Nominal Current rating can not be adjusted low enough to match the FLA of the motor being used.

Resolution:
The Nominal Current (nominal motor current) setting of the ATV66 series drives can be adjusted between .45 and 1.05 times of the nominal output current rating of the drive itself.
 
Was this helpful?
What can we do to improve the information ?