Technical FAQs

Ask a Question

How do you remove the power terminal cover on the ATV320 Compact version?

Issue:
How do you remove the power terminal cover on the ATV320 Compact version?

Product Line:
Altivar 320 compact

Environment:
All

Cause:
Installation Wiring

Resolution:
There is a padlock icon on the front lower portion of the drive.  You use a screwdriver to press on the tab in the hole at the padlock and the cover should pull forward to be removed for wiring or troubleshooting.
Was this helpful?
What can we do to improve the information ?