Technical FAQs

Ask a Question

What is the max lengthof the adjustable lever arm for XCKJ Limit Switch?

Issue:
What is the max lengthof the adjustable lever arm for XCKJ Limit Switch?

Product Line:
Heavy Duty / Industrial Metal Body

Environment:
XCKJ Operating Heads, Replacement Parts, and Levers

Resolution:
Roller arm can go as long as 3in, Rods can be as long as 8.4in. Please see the list:

ZCKY41 - Adjustable Delrin roller, 0.74 in. diameter, 0.2 in. wide, 3 in. long (max.)

ZCKY43 - Adjustable steel roller, 0.74 in. diameter, 0.2 in. wide, 3 in. long (max.)

ZCKY51 - Adjustable rod-square, steel, 1/8 in. side, 5.4 in. long (max.)

ZCKY52 - Adjustable rod-round, fiberglass, 1/8 in. diameter, 5.4 in. long (max.)

ZCKY53 - Adjustable rod-round, steel, 1/8 in. diameter, 5.4 in. long (max.)

ZCKY59 - Adjustable rod-round, plastic, 1/4 in. diameter, 8.4 in. long (max.)
Was this helpful?
What can we do to improve the information ?