Technical FAQs

Ask a Question

How do you properly connect or wire a transformer with the voltage code T75F?

Issue:
How is a transformer with the voltage code T75F wired or connected?

Product Line:
Transformer

Environment:
T75F transformers

Resolution:
For 480v delta to 240v delta.  
Connect 480v to H1, H2, H3, and cap off all other H wires individually.  
For 240V Delta connect X1, X2, X3 to the load. There are no options to derive a neutral. This is a delta delta configuration. See wiring diagram below.





 
Was this helpful?
What can we do to improve the information ?