Technical FAQs

Ask a Question

Is Form A20 Forward-Reverse pushbuttons momentary or maintained?

Issue:
Need to confirm the forward-reverse pushbutton on the NEMA Contactor/Starter is momentary or maintained

Product Line:
Reversing Contactors/Starters

Environment:
NEMA Contactors/Starters

Resolution:
Form A20 uses two black, momentary pushbuttons 9001KR1BH5.
Was this helpful?
What can we do to improve the information ?