Technical FAQs

Ask a Question

What does the S Suffix mean on ATV212HD22N4S drive?

Issue:
What does the S Suffix mean on ATV212HD22N4S drive?

Product Line:
Altivar 212

Environment:
All

Cause:
S-suffix

Resolution:
The S suffix is the slim version available for 22KW (30 HP) rating, IP 21 version.  It has a smaller dimensional footprint compared to regular ATV212 drive rated for 30 HP.
Was this helpful?
What can we do to improve the information ?