Technical FAQs

Ask a Question

Do we offer protection covers for the ZART12D?

Issue:Do we offer protection covers for the ZART12D?

Product Line:
Wireless Pendant Station

Environment:
ZAR Pendant Stations

Cause:
Product features and verification

Resolution:
The set of rubber protection is sold under different references depending of the color 
ZARC21 Green 
ZARC22 Red 
ZARC23 Blue 
ZARC24 Yellow 
ZARC25 Orange
we can now confirm that the ZARC2* part number include both the front and rear rubber protection.

Was this helpful?
What can we do to improve the information ?