Technical FAQs

Ask a Question

What conductor temperature is the MPPT60 rated for?

Issue:
Why does the MPPT60 recommend #6 AWG instead of #4 AWG which is rated for 85A at 75C?
Product Line:
MPPT60

Environment:
Pre-sales or during installation while choosing wire gauge

Resolution:
The MPPT60 is rated for the use of 90C conductor.

Cause:
The conductor rating for the MPPT60 is not mentioned in the electrical or mechanical specifications for the device.  However, there is a section that deals specifically with minimum wire gauge rating.  The information can also be found on the label on the side of the MPPT60.



Was this helpful?
What can we do to improve the information ?