Technical FAQs

Ask a Question

What is the part number for the charging motor assembly for the DC Switch (0J-530-2426) of an XCNA unit?

Issue:
Part Number for the charging motor assembly


Product Line:
XC, XCNA, SE1 series and some of the GT series

Environment:
Applications that use the XCNA units

Cause:
Charging motor assembly replacement

Resolution:
This component is a Square D part with the part# S48207
 
Was this helpful?
What can we do to improve the information ?