Technical FAQs

Ask a Question

Can I use the GT100 series inverters for Wind turbine applications?

Issue:
3phase inverters in wind applications

Product Line:

GT100, GT250, GT500 etc

Environment:
Applications that produce 3phase utility scale power

Cause:
Application modification for wind turbine applications

Resolution:
No, the units are only designed for Solar applications and can’t be modified to accommodate the wind turbine applications.


 
Was this helpful?
What can we do to improve the information ?