Technical FAQs

Ask a Question

What does the FA suffix mean on PowerPact circuit breakers?

Issue:
Meaning of -FA suffix on PowerPact Circuit Breaker

Product Line:
Circuit Breakers

Environment:
Applies to Powerpact M, P and R Frame

Resolution:
On a Powerpact M, P or R frame breaker, suffix 'FA' indicates the breaker has an 110-130Vac/dc UVR undervoltage trip, PLUS an adjustable time delay that can be set for 0.5, 0.9, 1.5 or 3.0 seconds before trip.
Was this helpful?
What can we do to improve the information ?