Technical FAQs

Ask a Question

Is the Valve assembly VB-7263-203-6-9 still available ?

Issue:
Is the Valve assembly VB-7263-203-6-9 still available ?

Product Line:
Valves and Actuators

Environment:
Ordering

Cause:
Cross reference

Resolution:

The assembly is not available , but ordering VB-7263-0-4-09 Valve,with AV-7400 Linkage kit, will provide the equal assembly parts
Was this helpful?
What can we do to improve the information ?