Technical FAQs

Ask a Question

What is the part number of the keps nut to hold the QOM1 and QOM2 main breaker into the load center?

Issue:
What is mounting hardware for QOM1 and QOM2?
 
Product Line:
Load Centers
 
Environment:
Applies to QO and HOM Load Centers

Resolution:
The part number for the keps nut used to tighten the QOM1 or QOM2 main breaker to the load center is 2342702001. A quantity of 2 are required for each QOM1 or QOM2 breaker.
 

Was this helpful?
What can we do to improve the information ?