Technical FAQs

Ask a Question

What is form X21 on part number 8502SBT3V02SX21 is?

Issue:
8502SBT3V02SX21 has form X21 and what does it mean.

Product Line:
Type S Contactor

Environment:
NEMA Contactors and Starters

Resolution:
Form X21 are 2 normally open and 1 normally closed auxiliary contact. System won't recognized the part with the said form. It needs to be built through product selector.
Was this helpful?
What can we do to improve the information ?