Technical FAQs

Ask a Question

What is the assembled part number for a VB-9313-0-5-12 valve, MA41-7150 actuator with AV-607-1 linkage kit?

Issue:
What is the assembled part number for a VB-9313-0-5-12 valve, MA41-7150 actuator with AV-607-1 linkage kit?

Product Line:
Field Devices

Environment:
Application

Cause:
Ordering

Resolution:
The assmebled Valle , actuator  and linkage will need to be ordered separately, the assembly is not available .
Was this helpful?
What can we do to improve the information ?