Technical FAQs

Ask a Question

Does QO260NATR come with a neutral?

Issue:
Is there a neutral kit available that can be used with QO260NATR?

Product Line:
Enclosed Molded Case Switch

Environment: 
Nema 3R molded case switch.

Resolution:
No, a neutral assembly is not supplied, however a ground bar kit is included. The device is suitable for 240 Vac loads only. For a 120/240 Vac application, consider a QO2000NRB. This also applies to QO200TR and QO200TRNM.

 
Was this helpful?
What can we do to improve the information ?