Technical FAQs

Ask a Question

What is the part number for Pneumatic tubing that has a 7/ 64" Interior wall diameter and 5/37 Outside diameter?

Issue:
What is the part number for Pneumatic tubing that has a 7/ 64" Interior wall diameter and 5/37 Outside diameter?

Product Line:
Field Devices

Environment:
Installation

Cause:
Ordering 

Resolution:
The Kele-T101 and 102 pneumatic tubing can be used , see attached for part numbers 
 
Was this helpful?
What can we do to improve the information ?