Technical FAQs

Ask a Question

What type of communication does the GT30 support?

Warning:
These instructions are intended for use by authorized service personnel who have training, knowledge, and experience in:
• Installing electrical equipment and PV power systems (up to 1000 V)
• Applying all applicable installation codes
• Analyzing and reducing the hazards involved in performing electrical work
• Selecting and using personal protective equipment
Perform LOTO to make sure all energy in the inverter is zero.  


Issue:
Communication methods for the GT30 unit.


Product Line:
GT30

Environment:
Applications that use the GT30 inverter

Cause:
Monitoring and communication methods for the GT30

Resolution:
The Xantrex GT30 can be remotely accessed through an RS232 serial port as shown in the figure below through an RS485/Modbus Connection.
The GT30 is also equipped with a full-duplex galvanically isolated RS232 serial port using a 9-pin, d-sub, connector


 
Was this helpful?
What can we do to improve the information ?