Technical FAQs

Ask a Question

Do any of the GT 3phase utility scale inverter meet the Hawaii HECO Rule 14H standard?

Issue: 
Hawaii code compliant requirements


Product Line:
GT100, GT250, GT500MVX, GT500-480

Environment:
Applications that use the 3phase GT units in Hawaii

Cause:
Do the inverters pass the HECO transient overvoltage test?

Resolution:
No these units do not meet the rule 14H settings as they are outside UL standards.
Was this helpful?
What can we do to improve the information ?