Technical FAQs

Ask a Question

Can we add an additional contact block for a 9001k37 Joystick?

Issue:
Can we add an additional contact block for a 9001k37 Joystick?

Product Line: 
Push Button Joystick

Environment:
North American Products

Cause:
Additional contacts for a Joystick 
Ex: 9001K37

Resolution:
Since the contact Blocks are separated all they need to do is to add additional contact to it
Was this helpful?
What can we do to improve the information ?