Technical FAQs

Ask a Question

Are MA-220 and MA-418-0-0-2 actuators still available for replacement ?

Issue:
Are MA-220 and MA-418-0-0-2 actuators still available for replacement ?

Product Line:
Valves and Actuators

Environment:
Maintenance

Cause:
Replacement 

Resolution:
The Fire /smoke damper actuator MA-220 from Barber Colman is obsolete , but calling the Damper mfg, and asking for a replacement is recommended.

The MA41-0-0-2 actuator is now available as revision 0-0-4. Order it as p/n MA-418. 
 
Was this helpful?
What can we do to improve the information ?