Technical FAQs

Ask a Question

ATV312 drive with a remote speed pot is working in reverse? 

Issue:
ATV312 drive with a remote speed pot is working in reverse? 

Product Line:
ATV312 

Environment:
All serial numbers

Cause:
Potentiometer is working backwards

Resolution:
Swap the +10V and the com termials wires to reverse the potentiometer direction.

 
Was this helpful?
What can we do to improve the information ?