Technical FAQs

Ask a Question

Why the XCNA inverter faulted on 0088 Too many online cycling?

Issue:
Inverter faulted on 0088 and would not clear
 
Product Line:
XCNA
 
Environment:
 
Cause:
It could be unstable grid, array issue or setting

Resolution:
Review the display values for grid voltage and PV Voltage and make sure that they are within the required parameters. If everything checked out fine then cycle AC power to see if the fault clear. Once it clear then enable to inverter and try to run. If the inverter ran, but not making any power even though the PV power was more than 10kwatts then call us at 866-519-1470 option 3 & 3. The unit is running in the CP mode and should have been in PV mode.
 
Was this helpful?
What can we do to improve the information ?