Technical FAQs

Ask a Question

What are the flash memory limitations on the SW/XW inverters?

Issue:
What are the flash memory limitations on the SW/XW inverters?

Product Line:
Conext SW/XW+ systems

Environment:
Remote control system in which the settings will be changed very often.

Cause:
Constantly changing settings

Resolution:
With modern firmware you don't have to worry about writing to the SW/XW+ flash ram. You actually now only write to a shadowed version of the config in DRAM. The shadowed version affects operation, but only gets written to the flash if you go into stb, or lose DC power. 
Was this helpful?
What can we do to improve the information ?