Technical FAQs

Ask a Question

Is the MP-485 actuator spring return?

Issue:
Is the MP-485 actuator spring return?

Product Line: 
Valves and Actuator

Environment:
Application

Cause:
Product Characteristics

Resolution:
The MP-485 actuator is not spring return and will stay in it's postion, in the event of a power failure.
Was this helpful?
What can we do to improve the information ?