Technical FAQs

Ask a Question

What is a good choice for a 1/2' 3W diverting/threaded/normally close/spring return valve can fit on an AG13B060Q1?

Issue: 
What would be a choice for a 1/2" (DIA) / 3W diverting / threaded (NPT) / normally closed (NC) / spring return valve, that can fit onto an AG13B060Q1 Actuator?

Product Line: 
Valves and Actuator

Environment:
Maintenance

Cause:
Replacement

Resolution:
The AG13B060Q1 Actuator is RESTRICTED to McQuay only 
The AG13B060Q1 actuator has a 96" lead length which is a special to McQuay.  The AG16B060 is available with 96" 
The VT3222 would be the correct valve , but getting it as an assembly with McQuay special actuator is not available , but valve VT3222 and actuator AG16B060, can be purchased separately and assembled in the Field .
Was this helpful?
What can we do to improve the information ?