Technical FAQs

Ask a Question

Where Can I Find Data sheets for the MPPT Output Breakers?

Issue
Where is some information available for the 865-1070 and/or 865-1080

Product Line
MPPT 60 150, MPPT 80 600

Environment
All MPPT installations using Schneider Electric recommended circuit breakers.

Resolution
See attached document.

Cause
Data sheets for the recommended MPPT output breakers are not available on the web site.  These particular circuit breakers are manufactured by Carling rather than Square D.
Was this helpful?
What can we do to improve the information ?