Technical FAQs

Ask a Question

Is there an enclosure available for Powerpact J frame breakers with GFM250JD ground fault modules?

Issue:
Is there a suggested enclosure size for breakers with GFM250JD ground fault module?

Product Line: 
Circuit Breaker

Environment:
ground fault module for Powerpact H frame breakers 

Resolution: 
No, we do not offer an enclosure that would accept Powerpact J frame breaker with an GFM250JD.  However the instruction bulletin, 48041-088-01, list recommended minimum size for customer sourced enclosures.
Minimum recommended size for standard 80% rated breakers would be 28.5 in. H x 12.38 in. W x 5.38 in. D.


http://download.schneider-electric.com/files?p_Doc_Ref=48041-088-01
Was this helpful?
What can we do to improve the information ?