Technical FAQs

Ask a Question

Is there an enclosure available for Powerpact H frame breakers with GFM150HD ground fault modules?

Issue:
Is there a suggested enclosure size for breakers with GFM150HD Ground fault module?
Product Line: 
Circuit Breaker

Environment:
Ground fault module for Powerpact H frame breakers 

Resolution: 
No, we do not offer an enclosure that would accept Powerpact H frame breaker with an GFM150HD.  However the instruction bulletin, 48041-088-01, list recommended minimum size for customer sourced enclosures.
Minimum recommended size for standard 80% rated breakers would be 18.13 in. H x 8.63 in. W x 4.13 in. D, for 100% rated breakers, 62 in. H x  22 in. W x  14 in. D 


http://download.schneider-electric.com/files?p_Doc_Ref=48041-088-01
Was this helpful?
What can we do to improve the information ?