Technical FAQs

Ask a Question

Is there an enclosure available for Powerpact J frame breakers with ELM250JD earth leakage modules?

Issue:
Is there a suggested enclosure size for breakers with ELM250JD, earth leakage module?

Product Line: 
Circuit Breaker

Environment:
 Earth Leakage ground fault module for Powerpact J frame breakers 

Resolution: 
No, we do not offer an enclosure that would accept Powerpact J frame breaker with an ELM250JD.  However the instruction bulletin, 48041-089-01, list recommended minimum size for customer sourced enclosures.
Minimum recommended size for standard 80% rated breakers would be 28.5 in. H x 12.38 in. W x 5.38 in. D, for 100% rated breakers, 62 in. H x  22 in. W x  14 in. D (ELM250JD is not certified for use with 100% rated 250A circuit breakers.)

http://download.schneider-electric.com/files?p_Doc_Ref=48041-089-01

 
Was this helpful?
What can we do to improve the information ?