Technical FAQs

Ask a Question

Does the VW3A3725 bacnet card have built in terminating resistors?

Issue:
Does the VW3A3725 bacnet card have built in terminating resistors?

Product Line:
VW3A3725 bacnet option card.

Environment:
All models, All serial numbers.

Cause:
N/A

Resolution:
No, the VW3A3725 Bacnet card does not have an integrated terminating resistor.  An external resistor of 120 ohms should be connected across the signal at each end of the daisy chain network.
Was this helpful?
What can we do to improve the information ?