Technical FAQs

Ask a Question

What's the difference between the MA-5210-002 and MA-5210-004 Actuators?

Issue:
What's the difference between the MA-5210-002 and MA-5210-004 Actuators? 002, and 004 are shown listed on labels

Product Line:
Field Devices

Environment:
Product Features

Cause:
Clarification

Resolution:
The  MA-5210-0-0-2 and the MA-5210-0-0-4 actuators are the same actuator , with the 002 and 004 suffix's, indicating an Engineering revision change.
It has nothing to do with the action or function of the actuator and should be ordered as MA-5210 only.
 
 
Was this helpful?
What can we do to improve the information ?