Technical FAQs

Ask a Question

Can I get a ET1.01 trip unit on a 4 pole P frame?

Issue:
Can I get a ET1.01 trip unit on a 4 pole P frame
 
Product line:  
Powerpact P frame
 
Environment:  
Powerpact P Frame
 
Resolution
The ET1.01 tip unit is not available on 4 pole P frame breakers. This trip unit is only available on 2 and 3 pole breakers.
 
Was this helpful?
What can we do to improve the information ?